FAQ: Can I do interleaved datalogging using the 14585A software or the ELOG commands?

No. Interleaved datalogging mode is only available from the N6705B front panel. The 14585A software and the ELOG commands cannot interleave the voltage and current measurements on power modules that do not have simultaneous V & I measurement capability.

Applies to: 14585A

Applies to: N6705A, N6705B

Select Home to return to the table of contents for more FAQs.

Visit our Power Products Forum for additional topics and discussions.

Read technical postings on our Power Blog – Watt’s Up?